Skip to content

Hydrogen System Design:                How It Differs from Oil and Gas 

About Hydrogen System Design

Social Media-FK Series Post4 FA

When designing fluid systems for hydrogen, it required a different approach as compared to the traditional oil and gas systems.

The reason is simple: hydrogen behaves differently. As the smallest molecules in the universe, it can permeate materials, escape through the tiniest leaks, and react in ways that demand special design considerations—making its unique properties impossible to ignore. 

To put it in perspective, if a hydrogen atom were the size of a golf ball, an oil molecule would be as large as the Earth. That’s how remarkably small hydrogen is—small enough to pass through microscopic gaps that oil molecules cannot. This is why precise sealing is not just important, but critical to safe, reliable system performance. 

At Swagelok Malaysia, we recognize the unique challenges of hydrogen systems and deliver engineered solutions that meet the demands of this evolving energy landscape. Our tube fittings are specifically designed to mitigate hydrogen leaks, addressing the issue of continuous pore structures—microscopic pathways between metal surfaces that hydrogen can permeate. The FK Series fittings are precision-engineered to minimize these leak paths, helping you maintain system integrity and safety. 

Components Matter: Why Tubing Wins in Hydrogen Systems

Tubing allows for more precise control of hydrogen flow. It’s lighter, easier to install, and better suited for the pressures when you are handling hydrogen. When you are working below 10,000 psi, Swagelok tube fittings are a reliable and trusted choice. Above that, some systems switch to cone and thread fittings—but those can be vulnerable to vibration and thermal changes.  

Designed specifically for demanding environments—including hydrogen applications—FK Series fittings offer robust performance up to 20,000 psig (1378 bar). They meet EC-79 standards for hydrogen use up to 700 bar (10,150 psig), and their vibration-resistant, leak-tight design helps protect both your system and your team. With a simple two-piece construction and preassembled cartridges, FK fittings install up to five times faster than cone and thread alternatives—reducing labor time, maintenance costs, and potential leak points.

Screenshot 2025-08-27 074117

Simple Pre-Assembled Cartridge Design

Screenshot 2025-08-27 074107

FK Fitting Complete Assembly

Line Sizing: Why Bigger Isn’t Always Better 

Line sizing is another area where hydrogen requires a different approach. While engineers often rely on calculators to determine the correct size for managing velocity and pressure drop, hydrogen’s behavior is unique. Its density changes with pressure—which can lead to inaccurate results if not properly accounted for. 

Oversizing components—a common habit among designers with oil and gas backgrounds—can significantly inflate costs. For instance, increasing from a ¾-inch to a 1-inch line can raise component costs by up to eight times. Right-sizing is not just efficient—it’s essential. 

At Swagelok Malaysia, our team of field engineer can work with you to size your system correctly, balancing performance and cost without compromising safety. 

Screenshot 2025-08-27 074129

Safety by Design: Keeping Hydrogen Secure 

The estimated flammability limit of this substance in the presence of oxygen is approximately 4%. To ensure safety, we maintain concentrations well below that level—typically around 1%. Any leaks that could cause accumulation near or above this level are considered a serious concern and must be addressed immediately. Consistency in system design is critical. Mixing technologies from multiple vendors, a common cost-cutting approach in oil and gas, can lead to maintenance challenges, operational inefficiencies, and increased risk of failure. 

Swagelok Malaysia offers a fully integrated portfolio of valves and fittings, ensuring compatibility, reliability, and long-term safety. Ready to optimize your hydrogen infrastructure? For more information, contact us at malaysiaenquiry@swagelok.com  

 

Swagelok FK Components for Priority Panel at H2 Refueling Station


Related Articles

Need more information, support, or quotation?

Give us a call at 603.8084.1818 or email us.